Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Running Code On Edge Without Redeploying Rauc

If you are trying to run a script or deploy a program to the edge board, you do not always need to redeploy the rauc bundle. The following steps outline how to deploy and run the program code:

  • Within Eclipse, save your code, then build and install the project.

Build and Install location in Eclipse

  • If using a VM, connect to Filezilla or plug in a USB drive.
  • Navigate to the projects 'Debug' folder within your file transfer, and transfer the program file to the '/tmp' directory of your SCADAPack. File transfer folders

  • Once the tranfer is complete, you can now SSH into the edge board --> navigate to the '/tmp' folder --> provide permission to the file:

chmod +x <filename>

  • You will now be able to execute the program. Note: Unlike the service, the code will only run once and only when executed; it will not automatically run on power up.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: