HDPM6000 head unit is not displaying current readings
Issue
The HDPM6000 head unit is not reading current even though the CT's are wired to the unit.
Product Line
HDPM6000
Resolution
The HDPM6000 head unit requires voltage connections as well as current connections in order to read properly. If only CT's are connected, the unit will not display values for current. Voltage must also be connected to the unit in order for the current to be read.
Released for: Schneider Electric Nigeria