Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Demonstrating Edge Forwarding Configuration on a SCADAPack 47xi

Edge Forwarding allows a user to access the Linux board while being connected to one of the RTU Ethernet Ports (ETH1 or ETH2)

For this example, Enable SSH Server (Edge Platform) under Ethernet >  Services.

Configuration tab > IP Communications> Services: SSH Service Enabled

ETH1 on SP474i was configured for 10.10.10.11 and Enable Edge Forwarding was checked off.

Ethernet 1 Settings: Enable Edge Forwarding checked off

The PC Ethernet port was configured for IP address 10.10.10.100 to be part of the same network subnet and it could ping ETH1 of the SCADAPack without issue.

Now, using Putty with SSH targeting the RTU board 10.10.10.11

Hot to setup Putty to access the Edge board

And with the Mode switch (rotary dial) set to F=PRVL, the user could log in as root using the appropriate password to access the Edge board.

Logging on to Edge board with SSH using Putty with rotary dial set to PRVL

If the Mode switch (rotary dial ) were set to 0=LOCAL, the user could attempt to login to the Edge board but access would be denied.

Putty connecting to Edge board with SSH - Mode set to LOCAL

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings