Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
APC Network Management Card (NMC) has no LED indicators or shows no power

Issue:
APC Network Management Card(s) installed in a compatible UPS, but neither the Link nor Status LEDs are illuminated.

Product Line:

  • Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
  • Network Management Card 3 (NMC3) - AP9640, AP9641, AP9643

Environment:
All Serial Numbers
All Firmware Revisions

Cause:
The NMC may not be receiving power due to several potential issues, including:

  • Loose connections or improper seating of the NMC.
  • A fault in the NMC hardware.
  • Firmware issues or corrupt settings.

Resolution:
1. Check UPS Status- Ensure the UPS is turned on and functioning properly. If the UPS is off, turn it on and check if the NMC powers up.

2. Inspect Connections -Remove the NMC and check for any visible damage. Ensure that it is properly seated in the SmartSlot of the UPS and it is secured with the provided screws.

3. Try a Different SmartSlot -If your UPS has multiple SmartSlots or if you have another UPS with SmartSlot for management cards, try inserting the NMC into a different SmartSlot to rule out a faulty connection. If the NMC functions properly in another UPS, you might want to upgrade your UPS's firmware by following the instructions provided in Schneider Electric KBase FA164737.

4. Try a Different NMC - If another known good NMC is available, swap the one in question by inserting it into the same SmartSlot in the UPS to help isolate the issue.

5. Format the Card (NMC2/NMC3 only) - Use a paperclip and press and hold the NMC's pinhole reset button for around 20 seconds. This will erase all user settings and configuration, including TCP/IP network settings.

6. Attempt to Update the NMC Firmware via XMODEM (NMC2/NMC3 only) - For step-by-step instructions on updating the NMC firmware through Terminal Emulation XMODEM, refer to Schneider Electric KBase FA156047.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings