How can we help you today?

How to downgrade the firmware to a previous version using Web in T300

This operation could be necessary for T300 version that have no longer USB port
used for backup/restore operation for example.
A firmware downgrade happens when the software's version number to be installed is less than the currently  Installed software, for example, from 2.9.1 to 2.9.0.
This functionality is present from 2.9 software version of PowerLogic T300.
When a downgrade is performed, the current configuration is lost to prevent a system malfunctioning.
This functionality requires a specific RBAC version that is not installed if the software version has been previously upgraded from 2.8 to 2.9. In this case, the required object included in CAE and security policy for 2.9 version, must be added.
This functionality is only available for users with SECADM role.

Downgrading the Software Version
Access via Maintenance > Advanced > Firmware

The system detects that the software version to install is lower than the current version. A message is displayed so that you can confirm the downgrade, or cancel it.

Click Install current new firmware version: V.V.V-date to continue the
downgrade. The same in Updated in User Manual from version NT00378–EN–12.pdf

Schneider Electric Nigeria