How can we help you today?

What is the internal power consumption of the Schneider OffGrid Portable Power Station when turned off or not in use?

Issue:

What is the internal power consumption of the Schneider OffGrid Portable Power Station when turned off or not in use?


Product Line:

Schneider OffGrid Portable Power Station

Environment:

All serial numbers

Resolution:

With the system turned off after 1 hr. (when LCD is off & no output is on), the power consumption in this state is under 0.5mA.

Schneider Electric Nigeria