Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Clearances for installing a PrismaSeT I switchboard in a room

Inside a switchboard there is heat dissipation from the devices and busbars in a normal running condition. This heat is dissipated out of switchboard mainly through the air circulation inside the switchboard by means of convection.

PrismaSeT I has rear panels which has louvers on top and bottom for an IP30/42 solution. These louvers allow the cold air to enter the switchboard from the bottom, absorb heat from switchboard, rise up and goes out through the top louver.

image 1

Incase of IP54 solution, this is taken care by forced ventilation

image 2

For this airflow to happen, it is essential the a gap is maintained between the switchboard and walls/roof while installation. Hence back to back assembly is not recommended with PrismaSeT I.

While installing a switchboard in a room it is recommended to maintain clearances for the reasons mentioned.

  • free space to enable for complete opening of the doors and operator access, maintenance or using a lifting device
  • Provide at least 600 mm of free space above PrismaSeT for incoming cable from top.
  • Sufficient space from rear of the panel to wall for the heat dissipation from the switchboard.

Also, recommendations from local regulations shall be taken care.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings