How can we help you today?

Symmetra 1 Phase: Not For Consumer Use Sticker

Issue:
Symmetra Packaging has sticker saying 'Not For Consumer Use'

Not for consumer use

Product Line:
Symmetra LX, Symmetra RM

Environment:
All serial ranges

Cause:
The Symmetra LX/RM product line is designed as a category C2 UPS product, which are typically used for non-residential environments. In a residential environment, this product may cause radio interference, in which case the user may be required to take additional measures.
In practice, there are no known issues with a Symmetra product causing interference for security systems or other common systems used in residential, commercial, or industrial spaces. Therefore, Symmetra are considered to be safe for use throughout Europe.

Resolution:

An official letter has been written with the above wording to alleiviate any concerns.

Schneider Electric Nigeria

Attachment(s)
Symmetra Use in Europe.pdf [130.22 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings