Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which IIS components and .NET framework are required for Machine SCADA Expert v2023 Mobile Access to work properly?

Issue:

If the required ISS components and .NET framework are not installed, mobile access will not function correctly in Machine SCADA Expert.

Product:

Machine SCADA Expert v2020/v2023.

Environment:

HMI Configuration Software in Windows

Resolution:

Attached to this FAQ is a PDF file with the components required for Mobile Access to function properly and some additional information.

Schneider Electric Nigeria

Attachment(s)
EMSE_WEB_IIS_V3_01_17_2025.pdf [479.46 KB]