Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to display DNP3 and/or Modbus protocol addresses in Logic Editor?

If you added DNP3 point numbers and/or Modbus register addresses before selecting the Object Protocol Address(es) in the Logic Editor custom field, you can display those addresses in the SCADAPack x70 Logic Editor:

  1. Go offline in RemoteConnect.
  2. Under My Network, right-click on SCADAPack x70 Controller Settings-DeviceDTM and select Additional Functions>Project Settings.

Display1

  1. Select the Object Protocol Address(es) in Logic Editor Custom Field checkbox.

Display2

  1. Click Ok.
  2. A window will pop up " The Project Settings have been updated. Click the View log File button to see the complete list of changes". and select Close button.

Display3

  1. Open Logic Editor
  2. Under Project > Variables & FB Instances, double click on Derived Variables and view Custom field.

Display4

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings