Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Programming a digital input for fault reset on an ATS480 softstart?

Navigate under Menu 4 inputs/outputs menu.

Find Di3 and DI4 assignments.

The preferred input can be programmed as fault reset (LIRSF). This will allow the device to clear a detected error with the toggle of a contact made between DI3 or DI4 to 24V terminal.

fault reset