Can I connect to Twido PLC using EcoStruxure Machine Expert Basic?
Issue:
I know that Machine Expert Basic can open and convert a TwidoSuite project file, but can Basic actually connect to and upload from a Twido?
Product Line:
Twido PLC
Environment:
EcoStruxure Machine Expert Basic
Cause:
N/A
Resolution:
Ecostruxure Machine Expert Basic can open and convert a Twidosuite program, but is used only to connect to M221, M200, M100, TM3 and TM2 modules.
Released for: Schneider Electric Nigeria