Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME 2024- Tamper detected error. A valid software license could not be found.

Product Line
Power Monitoring Expert 2024
_____________________________________________________________
Environment
License Configuration Tool
_____________________________________________________________
Issue :
A valid software license could not be found.
A valid license could not be found

The system logs are flooded with the error: Tamper detected: FlxDotNetClient.SvcSessionException: MID=0, SID=0, EID=6

_____________________________________________________________
Proposed Solution

Solution 1:

Import the attached certificates into the Trusted Root Certification Authority through the Manage Computer Certificates interface.

  1. VeriSign Universal Root Certification Authority.cer
  2. VeriSign Class 3 Public Primary Certification Authority - G5.cer
  3. DigiCert Trusted Root G4.cer
    Trusted Root Certification

    Then Run the below PowerShell script after getting the exported certificate in the system.

    Change the path of the exported file in the following script and run it in PowerShell ISE in administrator mode.

    $sst = ( Get-ChildItem -Path C:\certs\roots.sst )

    $sst| Import-Certificate -CertStoreLocation Cert:\LocalMachine\Root

    Solution 2:
    If the previous solution fails, rebuild the certificate chain from a functioning PME system.
    From a working PME system, export the three previously stated certificates.
    Here is the link to exporting the trusted root certificate from the working machine.
    http://woshub.com/updating-trusted-root-certificates-in-windows-10/

    Then run the below PowerShell script in the non-working system after getting the exported certificate in the system:

    Change the path of the exported file in the following script and run it in PowerShell ISE in administrator mode

    $sst = ( Get-ChildItem -Path C:\certs\roots.sst )

    $sst| Import-Certificate -CertStoreLocation Cert:\LocalMachine\Root

Schneider Electric Nigeria

Attachment(s)
VeriSign Universal Root Certification Authority.cer [1.18 KB]
VeriSign Class 3 Public Primary Certification Authority - G5.cer [1.21 KB]
DigiCert Trusted Root G4.cer [1.39 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings