Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
IGP10-T 4 and 20 mA Loop Check
  1. Press the NEXT button 3 times and CALIB will be displayed
  2. Press ENTER and CAL ATO will be displayed
  3. Press NEXT 3 times and ADJ 4mA will be displayed
  4. Press ENTER and A 4mAΔΔ will be displayed. At this time the transmitter output will be locked at 4mA.
  5. When 4mA loop check is done, press NEXT 5 times and ADJ20mA will be displayed
  6. Press ENTER and A20mAΔΔ will be displayed. At this time the transmitter output will be locked at 20mA.
  7. When 20mA loop check is done, press NEXT 6 times and CANCEL will be displayed
  8. Press ENTER and transmitter will return to measurement mode.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings