How can we help you today?

What is the default IP address of the Edge I/O network interface module NTSNEC1200?

Issue:

Default IP address of the Edge I/O network interface module NTSNEC1200

Product Line:

Edge I/O, NTSNEC1200

Resolution:

The default IP address of the Edge I/O NTSNEC1200 is 10.10.x.y where x.y is the last two octets of the MAC address converted to decimal.

Example:  If the MAC address is 00.80.F4.02.EA.6A then the IP address will be 10.10.234.106

EA Hex = 234 Decimal
6A Hex = 106 Decimal

Schneider Electric Nigeria