Link150/EGX150 - How to remotely power cycle
Issue
During troubleshooting, there may be a need to power cycle a Link150 gateway remotely. Power cycling the gateway releases existing connections which can allow other software to communicate to the 7801 port for example, which only allows 1 connection at a time.
Product Line
Link150/EGX150
Environment
Link150 Web Server
Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.
1. Log into the Link150 web page. Refer to https://www.se.com/us/en/faqs/FA299649/ for the default login information.
2. Navigate to the Settings tab > Communication > IP Network Services:
3. Check or uncheck the box to enable ION Pass Through, then click Apply Changes. The Link150 will reboot.
4. Refresh the page and log back into the Link150 web server.
5. Repeat the above steps to set the ION Pass Through back to its previous setting, which will reboot the Link150 again.
Released for: Schneider Electric Nigeria