Issue
Can the firmware for the VarPlus Logic VL 6 be upgraded?
Product Line
VarPlus Logic
Environment
Firmware
Resolution
The VarPlus Logic VL6 firmware is not field-upgradable. The current firmware version is 001.000.002.
Released for: Schneider Electric Nigeria