How can we help you today?

When configured with multiple vSAN clusters, PowerChute Network Shutdown fails to disable HA and vCLS all the clusters.

Issue:

PowerChute Network Shutdown has been configured to shutdown multiple vSAN clusters and HA/vCLS is only disabled on one cluster.

Product Line:

PowerChute Network Shutdown versions 5.0, 5.1, 5.2

Environment:

VMware vCenter 7 or 8 configured with multiple vSAN clusters.

Cause:

PowerChute can only disable HA and power off vCLS for a single cluster.

Solution:

Install multiple instances of PowerChute. One for each cluster.

Schneider Electric Nigeria