How to Install a Smart UPS Ultra Modular into a 2-Post Rack
Issue:
Installation of a Smart UPS Ultra Modular into a 2-post rack
Product Line:
Smart UPS Ultra Modular 1PH
Environment:
All serial numbers (Global)
Resolution:
NOTE: The 2 post mounting brackets (SRYLOPT2 for mounting UPS Frame and SRYLOPT5 for mounting the XBP frame) are available as an accessory and should be procured separately.
The APC Smart-UPS Modular Ultra, an Uninterruptible Power Supply (UPS), is designed for easy installation in a 2-post mount.
Models With UPS Frames Only:
Models with both UPS and battery frames
You may also refer to the attached manual (refer to page 23 onwards).
If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.
Released for: Schneider Electric Nigeria