How can we help you today?

Is it ok to turn off my UPS when not in use?

Question:
Is it ok to turn off my UPS when not in use?

Scenario:
APC by Schneider Electric notes that this question is often asked by our customers who would want to make sure there are no electronics that are on while they leave their homes or their place of work/business. It can also apply to times of expected power outages or electrical testing to be done at their areas.

Product Line:
All 1PH APC by Schneider Electric UPS units - All INDOOR - Plugged in models - All Serial Numbers

Resolution:

As long as the UPS is getting adequate power or it is plugged in to a good power source, then it will be ok.

If this is something we cannot avoid then please keep the following bullet points in mind.

  • Make sure all batteries are disconnected from the UPS before unplugging them.
  • Make certain we always recall FAQ FA156516. Although this FAQ does state that the minimum is 3 months (as per environmental conditions). APC by Schneider Electric deeply advises that this is NEVER done repeatedly as this can lead to batteries dying earlier than expected. Failure to follow the mentioned FAQ may cause the batteries to discharge completely and can result to them failing prematurely.
  • Portable Power Stations (PPS330, PPS500, PPS730) are designed to hold a charge for prolonged periods of time. Please refer to FAQ000271771 for the discharge rates of these offers. They will only use their port power only if they are on and with a load being fed.

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: