How can we help you today?

What value is expected when measuring capacitance of individual capacitors in a Powerlogic PFC capacitor bank?

Issue:

It may not be clear what value is to be expected when measuring capacitance for capacitors in a Powerlogic PFC capacitor bank.

Product Line:

Powerlogic PFC capacitors

Resolution

There will be a uF rating on the label of the capacitor. The L-L measurement taken should be 1.5X the value printed on the capacitor label. The photo below shows a typical label and where this value can be found.

Individual Capacitor label example

Example: BLRCH292A350B57, the capacitance per phase for this capacitor is 93.8uF.  93.8 X 1.5 =140.7uF

You would need to measure line to line (A to B, B to C, and C to A) on the capacitor and the values should be around 140uF -/+5% for each measurement.

Schneider Electric Nigeria
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings