Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What should I check if I can't change the mode on the XVR3 series ?

The possibilities are as follows:
- The mode setting may be incorrect.
Please check the rotary switch mode setting based on the instruction sheet.
- The rotary switch may be physically damaged.
The rotary switch will break if pressed too hard when changing modes.

Have a look at the pictures in attachment.

If the above does not resolve the issue, remove the product from the control device and check the product alone.
If it still does not work, the product may be broken.

Schneider Electric Nigeria

Attachment(s)
FAQ XVR3 - 1.pdf [233.18 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: