Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
IDP10-A Flow Configuration
  1. Press NEXT 2 times. The word CONFIG will be displayed
  2. Press ENTER, OUTDIR will be displayed
  3. Press NEXT and display will show OUTMODE
  4. Press ENTER then press NEXT until LINEAR is displayed and then press ENTER Display will now indicate OUTFAIL
  5. Press NEXT 2 times. Display will indicate DISPEGU
  6. Press ENTER and display will indicate USE EGU
  7. Press ENTER Display will indicate EGU SEL
  8. Press ENTER then press NEXT until INH2O is displayed the press ENTER. Transmitter will now display EGU LRV.
  9. Press ENTER and current lower range value will be displayed.
  10. Press ENTER and the left hand most digit will blink. Press NEXT to increment this digit by one until it is a 0. When the digit is at 0, press ENTER and repeat steps with the remaining digits.
  11. After the last digit is edited, press ENTER. Display will now indicate SET DP
  12. Press the NEXT button until the decimal point is in the desired location the press ENTER.
  13. Display will indicate EGU URV.   The EGU URV is the differential pressure upper range value.
  14. Press ENTER and current upper range value will be displayed.
  15. Press ENTER and the left hand most digit will flash. If the digit needs to be changed press NEXT to increment this digit by one. When the digit is at the desired value, press ENTER and repeat steps with the NEXT digit.
  16. After the last digit is edited, press ENTER. Display will now indicate SET DP
  17. Press the NEXT button until the decimal point is in the desired location the press ENTER.
  18. Display will indicate CANCEL.
  19. Press NEXT and display will indicate SAVE.
  20. Press ENTER and display will momentarily display SAVING and the return to the measure mode indicating pressure in INH2O
  21. Press NEXT 2 times. The word CONFIG will be displayed
  22. Press ENTER, OUTDIR will be displayed
  23. Press NEXT 2 times. Display will show OUTMODE
  24. Press ENTER the press NEXT until SQ<1CUT is displayed and the press ENTER Display will now indicate OUTFAIL
  25. Press NEXT 2 times. Display will indicate EGU SEL
  26. Press ENTER and display will indicate PCTSQRT with the letter “P” flashing. This is where you enter the Flow Engineering Unit. The letters can be edited by pressing the NEXT button. This will increment the letters through the alphabet.
  27. Once the desired label has been entered the next display will indicate DSP URV
  28. At DSP URV press enter and current Flow Upper Range Value will be displayed.
  29. Press ENTER and the left hand most digit will flash. If the digit needs to be changed press NEXT to increment this digit by one. When the digit is at the desired value, press ENTER and repeat steps with the NEXT digit.
  30. After the last digit is edited, press ENTER. Display will now indicate SET DP
  31. Press the NEXT button until the decimal point is in the desired location the press ENTER.
  32. Display will indicate CANCEL.
  33. Press NEXT and display will indicate SAVE.
  34. Press ENTER and display will momentarily display SAVING and the return to the measure mode indicating flow in the selected engineering unit.
  35. COMPLETE

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: