EGU LRV = 4 mA Value
EGU URV = 20 mA Value
- Press the NEXT button twice and the word CONFIG will be displayed.
- Press ENTER and OUT DIR will be displayed
- Press NEXT 4 times and DISPEGU will be displayed
- Press ENTER and USE EGU will be displayed
- Press ENTER and EGU SEL will be displayed
- Press ENTER and the current engineering unit will be displayed
- Press NEXT until the desired engineering unit is displayed (i.e. FtH2O, inH2O, PSI...)
- When desired engineering unit is displayed, press ENTER and EGU LRV will be displayed
- Press ENTER and the cursor at the left side of the display will flash.
- Press ENTER and the left hand most digit will flash.
- Press NEXT until this digit matches the value of the most significant digit of the desired LRVvalue. Repeat procedure for the remaining 3 digits until the entire LRVvalue has been entered
- Press ENTER and SET DP will be displayed
- Press NEXT until the decimal point is in the correct location
- Press ENTER and EGU URV will be displayed.
- Press ENTER and flashing cursor will appear at the left side of display
- Press ENTER and the left most digit will flash
- Press NEXT until this digit matches the value of the most significant digit of the desired URVvalue. Repeat procedure for the remaining 3 digits until the entire URVvalue has been entered
- Press ENTER and SET DP will be displayed
- Press NEXT until the decimal point is in the correct location
- Press ENTER and CANCEL will be displayed
- Press NEXT and SAVE will be displayed
- Press ENTER and device will be returned to Measurement Display
- Complete
Released for: Schneider Electric Nigeria
Discontinued
Discontinued
Discontinued
Discontinued