How can we help you today?

How to view the real time logic address of Altivar Drives?

Issue:

How to view the real time register or bits within these Input and Output Scanner Modbus Registers?

Product Line:

ATV630, ATV930, ATV340

Environment:

All serial numbers

Cause:

This has to do with troubleshooting capabilities.

Resolution:

In SoMove, there are three options to see the values of registers.

1) Under Display -> Communication Mappings

SoMove_1

2) The second option is to create your own display by clicking on "Motor" and "Drive" then highlight and pull the registers to the empty space to create your own display.

SoMove_2

The third option is to add the parameter for visualization on Dashboard/Display section, by its Logical Address - example is LFRD:

SoMove_3

For legacy drives like ATV61/71/320 - the feature in SoMove is not available.

Schneider Electric Nigeria