Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Key differences between the AP9613 and AP9614

Topic:

Key differences between the AP9613 and AP9614

Product Line:
AP9614, AP9613

Environment:
All serial number (Global)

Resolution:

The APC by Schneider Electric has released last  Jan. 20, 2025 its new Dry Contact I/O card (AP9614) introducing several improvements compared to the previous model, AP9613.  Dry Contact I/O card (AP9613).

  1. The AP9614 now includes a built‑in Web GUI, allowing users to configure UPS settings and define actions based on status changes or UPS events directly through the interface. For more information, please refer to FAQ000273840
  2. The AP9614 supports easy firmware updates via the Web GUI, streamlining maintenance and reducing the need for manual processes.
  3. The new model uses a Micro USB interface, enabling faster and more efficient data transfer, compared to the Mini USB connection used in the AP9613.
  4. The AP9614 can be readily identified through its updated pin configuration and internal components, offering clearer differentiation from the AP9613.

AP9614 vs. AP9613

(AP9614)                                                             (AP9613)

If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: