How to download an Event Log file from an AccuSine
Issue: The Event Log from the AccuSine is often requested in order to troubleshoot recurring events on the device. The following process outlines the steps to download the entire event log to a USB flash drive so it can be analyzed by technical support.
Product Line
AccuSine PCS+
AccuSine PCSn
AccuSine EVC+
Resolution
A USB flash drive will be needed in order to download the event log from the AccuSine.
The flash drive needs to be formatted to the FAT32 storage type. The following steps are provided to format the drive to FAT32 in case it is not already formatted to FAT32. These instructions are for Windows PC's. If the drive is not formatted to FAT32, it could cause errors to occur when downloading the event log.
Note: Formatting the USB drive will erase all data on the drive.
- Connect the drive to your computer.
- Open File Explorer and navigate to "This PC".
- Right-click on the drive you want to format and select "Format".
- Choose "FAT32" from the "File system" dropdown.
- Click "Start" to begin the formatting process.
-
Once the drive has been formatted, insert the USB drive into the USB-A port below the HMI or into one of the USB-A ports on the back of the HMI.
-
Use the HMI to navigate to the Event Log
-
Once the event log is displayed, select the folder icon with a downwards facing arrow to save a copy of the event log onto the USB drive.
-
A message will display stating that saving the Event Log requires a device plugged into the HMI USB port. Select "Continue"
-
Once the Event Log is saved, a message will display indicating the Event Log has been saved successfully.
-
The Event Log can now be sent to technical support for evaluation.
Released for: Schneider Electric Nigeria