Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M580 Hot Standby Device DDT type : T_M_ECPU_HSBY vs T_M_ECPU_HSBY_EXT

Issue :

When working with M580 Hot Standby application, why do I sometimes see the Device DDT type T_M_ECPU_HSBY and other times T_M_ECPU_HSBY_EXT

Products :

Control Expert (Unity Pro)

M580 Hot Standby

Answer :

This is based on the application level of your application.

If you have an application defined with an M580 of 2.70 and lower, you will see the T_M_ECPU_HSBY.

M580 2.70

If you have an application defined with an M580 of 2.80 and higher, you will see the T_M_ECPU_HSBY_EXT.

M580 2.80

In the PDF attached the differences between the 2 types have been identified.

Schneider Electric Nigeria

Attachment(s)
M580 Hot Standby Device DDT differences.pdf [182.82 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: