Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When migrating a Quantum Hot Standby to M580, why don't I see the choice of a M580 Hot Standby in the CPU choice

Product :

Unity Quantum Hot Standby

M580

Control Expert

UMAC (Unity M580 application converter)

Issue :

When migrating a Quantum Hot Standby to M580, why don't I see the choice of a M580 Hot Standby in the CPU choice. It only shows me the P584040, P585040 and P586040.

Solution :

Check in your Quantum application if there is a specialty task (AUX0, AUX1, Timer Events, I/O events).

Quantum task

Those are not supported by the M580 Hot Standby and that is why the UMAC tool does not give you an option for those CPUs.

The Analysis of the .ZEF file will show this.

UMAC analysis

The Quantum application must be modified to remove those specialty tasks before being processed by the UMAC tool.

Once this is done, the M580 Hot Standby CPUs will show up as a selectable option.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings