Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to power cycle an InRow unit Generation 1?

Issue:

How to power cycle an InRow unit Generation 1?

Product Line:

InRow Family Gen1.

Environment:

ACRD1XX, ACRD2XX, ACSC1XX, ACRC1XX, ACRD5XX, ACRP1XX, ACRP5XX, etc.

Cause:

General aid for Customers.

Resolution:

  1. Please put the unit into StandBy mode (Figure 1), you might be required to input the password, use the default oneà apc (lower case).

Path in a display

Figure 1

  1. When the fans start ramping down, please unplug the dedicated power cord(s) to the unit (It can be top or bottom fed) [Figure 2] or put down the dedicated breaker(s) to the unit (If it’s hard-wired), or if it’s a 600mm InRow (Figure 3) and leave the unit without any power for at least 5 minutes.

Inrow unit

Figure 2 (For 300mm InRow only).

Inrow unit 600 mm

Figure 3 (For 600mm InRow only).

  1. After the 5 min passes, restore the power to the unit, allow a couple of minutes, for the display to pop up, change the mode from StandBy to On (Figure 4), and test the proper operation of the unit.

Display path

Figure 4

NOTE: This process can only be executed from the front display of the unit.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings