Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is TM3 Haz Loc Certification meaning Class I Div 2 ?

Issue:

Is Haz Loc Certification of TM3 meaning Class I Division 2 environments?

Product Lines:

TM3 modules

Environment:

All model numbers

Resolution:

Yes, The Haz Loc Certification means approval for using in explosive environment Class I Div2.

This is a certification from UL, in file E361380. UL logo, together with Class I, Division 2, Group ABCD and this File number is also marked on the product.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: