Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Changing the Edge Password on SCADAPack 474i and 470i.

Maintaining the security of SCADAPack 474i and 470i devices is critical, particularly when managing remote access. One essential security measure is updating the Edge password. This document outlines the procedure for changing the Edge password using SSH access through PuTTY.

Prerequisites

Before proceeding, ensure the following:

  • PuTTY is installed on your workstation. PuTTY is a free SSH and telnet client available for Windows.
  • Network access to the SCADAPack device is established. This can be achieved via:
    • USB connection using IP address 10.2.3.4
    • Ethernet connection through the ETH3 port

Procedure

  1. Launch PuTTY and configure the session:
    • Set Connection Type to SSH
    • Enter the Host Name (or IP address) as 10.2.3.4 (for USB connection)
    • Leave the Port set to the default value 22
    • Click Open to initiate the SSH session
  2. Authenticate using the current Edge credentials.
  3. Once logged in, execute the following command to initiate the password change: passwd
  4. The system will prompt you to enter the new password.

Putty command

Password Recovery

If the Edge password has been lost or forgotten, it cannot be recovered. In such cases, the password can be reset by performing a factory boot on the device.