Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Disabling TLS 1.3 in Geo SCADA Expert (August 2024 Update and Later)

⚠️*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system.
Always backup the registry before making any changes.*

Starting with the Geo SCADA Expert August 2024 update, a new registry setting was introduced that allows users to disable TLS 1.3 specifically for Geo SCADA, without impacting the system-wide TLS configuration managed by Schannel.

To (temporarily) disable TLS 1.3 on a Geo SCADA server, follow these steps:

  1. Open the Registry Editor (regedit).
  2. Navigate to the following key:
    HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\SCXCom
  3. Create a new String Value named:
    EnableTLS13
  4. Set its value to:
    - "False" to disable TLS 1.3
    - "True" to enable TLS 1.3 (default behavior)

Note: This registry key is not created automatically. If it is missing, Geo SCADA will treat it as "True" by default.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: