ETE - FAQ - Offer: How will the EcoStruxure Transformer Expert solution aid transformer Asset Managers?
The EcoStruxure Transformer Expert solution is an advanced tool that provides the insulation health status of a transformer in an easily accessible format. This information will enable Asset Managers to extend the life of aging transformer assets by determining the risks of increasing load or continuing to operate a transformer, as well as making informed decisions on when to refurbish, which maintenance strategy to apply, and when to replace. With fleet-wide reporting, transformers can be easily ranked based on Life Left, Hot Spot Temperature and Water Content of Paper.
Released for: Schneider Electric Nigeria