Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Transformer: What is a substation transformer and what are do's and don'ts of safety precautions?

The substation transformer is static equipment, which converts electrical energy from one voltage to another. As the system voltage goes up, the techniques to be used for the design, construction, installation, operation, and maintenance also become more and more critical. Please visit Substation Transformer Basics to learn more.