How can we help you today?

ETE - Knowledge - Sensor: EcoStruxure Transformer Expert with H2 Dual Sensor

The EcoStruxure Transformer Expert with H2 Dual Sensor is our standard sensor with an add-on Hydrogen sensor. The additional hydrogen sensor is connected to the probe with help of the H2 Option Dual Splitter.


See the Installation and Commissioning Guide for more information.

This product is available for market release. A sample Hydrogen sensor model is displayed below.

ETE H2 Dual

ETE H2 Dual

ETE H2 Dual

ETE H2 Dual

Please see datasheets attached at the bottom of this article for more information.

Schneider Electric Nigeria

Attachment(s)
FAQ000276015 - H2Scan-Gridscan-Brochure-2020.R3_4pg.pdf [1.35 MB]
FAQ000276015 - EcoStruxure-Transformer-Expert_H2_Datasheet.pdf [1.08 MB]