Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Transformer: What test results indicate normal operation and what can indicate a fault?

If the water content in the transformer oil is within the IEEE standard specified limits, then, we can be comfortable with its operating condition. Violating the standard limits may result in fault conditions. The same applies for temperature measurements.

The EcoStruxure Transformer Expert solution provides the exact data for temperature as well as the water content in oil and hence indicates normal or risky operating conditions.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings