Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Logger: EcoStruxure Transformer Sensor Power Supply Specifications

The EcoStruxure Transformer Sensor operates at 18 - 42VDC, however, it is provided standard with a 110/240 VAC to 24 VDC, HDR-15-24 DIN rail mount power adapter, as shown below:

Power Supply

A suitable power source will need to be identified for the installation of this device. Schneider Electric will provide 10m low voltage cabling, with a pre-installed 5-pin M12 connector, for connection to the logger. Please ensure that the LV cable meets internal standards. The schematic below shows the power connections for the EcoStruxure Transformer Sensor and power supply.

Schematic

Schneider Electric Nigeria

Attachment(s)
HDR-15 Datasheet.pdf [703.3 KB]