Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How are the ATV320 Function Block Identification Fbi- parameters used?

Response:

Understanding Fbi-

Fbi 1

These parameters are populated as Function Block Logic is added to the ATV320 Logic Configuration in software like SoMove:

For Example:

Fbi 2

BVER is the Program Version:

Fbi 3

Fbi 4

BNS is the Program Size:

Fbi 5

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)