Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Geo SCADA: MQTT driver - 'Reason' parameter for JSON, Text and Sparkplug

Question

If the MQTT driver in Geo SCADA loses connection to the  MQTT broker or data point for a period of time (I.E. 30 minutes), upon reconnection, MQTT will send a backfill payload along with the current value.  Geo SCADA handles this well, but in history, all data is reflected as ‘Current Data’.  Is it possible to change the reason code for the backfill data so that a user may discern between current vs backfill data?

Answer

The reason for logging is different for each MQTT driver (see below):

JSON Schema A: Reason is 'Report' except if the message type is an alarm (I.E. has "status") in which case it is 'Value Change' for analog/counter points, and 'State Change' for digital points.

Text: Reason is always 'Current'

Sparkplug: Reason is 'Value Change' for analog/string/time points and 'State Change' for digital points


At the MQTT level, Geo SCADA just receives payloads from a broker.  Geo SCADA does not know when they were sent or whether they were queued up in the broker.  A device that is publishing data may publish multiple payloads, one after the other.  This would look the same to Geo SCADA as receiving multiple payloads when Geo SCADA connects.

The device that is publishing the data does not know if Geo SCADA is connected or not.  As the payload typically does not have a means of indicating whether the data should be considered historical or not, Geo SCADA has no recourse to categorize it any differently to data that is collected via a typical connection.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: