Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use a ZBRA1-active antenna with the EcoStruxure Panel server?

Yes, ZBRA1 active antenna can be used with the EcoStruxure Panel server. However, ZBRA1 is not compatible with PowerTag field device.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: