What is the default user name and password for the TM5 Ethernet/IP fieldbus interface module?
Issue:
Default user and password for the TM5 Ethernet/IP interface module
Product Line:
TM5NEIP1
Resolution:
When logging in to Web server for the first time, the default username is admin and the default password is TM5NEIP1. The user is requested to change the password.
NOTE: The only way to gain access to a TM5 EtherNet/IP Fieldbus Interface for which you do not have the password is by performing a Fieldbus interface clear flash memory operation (rotary switch position F0).
(see attached Modicon TM5 EtherNet/IP Fieldbus Interface, Hardware Guide page 37)
Released for: Schneider Electric Nigeria