How can we help you today?

Is a recovery USB available for PSA6 ?

No, recovery USB is not available to be purchased.

The user can create a recovery USB from the Recovery Utility feature provided on the HMIPSA6 Launcher.

Prepare a commercially available USB memory with a size of 32 GB or more, to create a recovery USB and follow the steps below:

  • 1. Disconnect all connected devices from the product.
  • 2. Insert a commercially available USB memory.
  • 3. Open the Launcher on the desktop.
  • 4. Select the Recovery USB icon.
  • 5. Select the USB memory in Select a disk menu.
  • 6. Select Start.
  • 7. In the confirmation screen, select OK.
  • 8. When completed, select OK.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings