Can the BMXNOR0200H module's Ethernet communication be reset using IO_DDT (ETH_RESET)?
1. Issue
Some customers have reported that the online help in Control Expert suggests BMXNOR0200H supports Ethernet communication reset via IO_DDT (ETH_RESET). However, this functionality is not supported. The only available method to reset the Ethernet communication is through the module’s web interface.
2. Product Line
-
Module: BMXNOR0200H
-
Software: Control Expert
3. Environment
-
Operating System: Windows 10 / Windows 11
-
Software: Control Expert
-
Browser: Any standard browser used to access the module’s web interface
4. Resolution
After consultation with R&D, it has been confirmed that BMXNOR0200H does not support Ethernet reset via IO_DDT. The only supported method is through the web interface of the module.
Note:
No updates to the user manual are planned. It is recommended to use the BMENOR2200H (Advanced RTU module) instead, which supports Ethernet reset via Device DDT.
Released for: Schneider Electric Nigeria