Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SAGE RTU – Lost Password Recovery Options on Secure Firmware

Issue:

User has lost or forgotten the password for the SAGE RTU 3030M unit.

Product:

SAGE RTU

Environment:

Secure Firmware-enabled SAGE RTU devices.

Cause:

Passwords cannot be recovered due to the secure firmware design, which prevents unauthorized access and ensures system security.

Resolution:

There is no way to recover the existing password. The available options are:

  1. Send the RTU´s CPU to Schneider Electric

    • We will restore the USER account file to default (as if a new CF card was purchased).
    • The RTU will be out of service until the restored CF card is returned.
    • Benefit: The existing configuration will be retained and will work as before once reinstalled.
  2. Purchase a new CF card, part number C3414-S02-10001

    • This allows the RTU to remain in service until the new CF card arrives.
    • The new CF card will have a blank default configuration and default user account (“Admin/Telvent1!”).
    • The customer must reinstall their configuration file. If no backup exists, the configuration must be re-entered manually.
  3. Manual restoration using a CF card reader

    • Restore the default USER account and extract the configuration from the old CF card to the new one.
    • Not recommended for field repair as it is easy to corrupt the CF card, making it unbootable.
    • This is the same process Schneider Electric performs in the lab when option 1 is chosen.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings