Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SAGE RTU CPUs — CF/PCMCIA Card Compatibility and Boot Sector Requirement

Issue:
Standard off‑the‑shelf CompactFlash (CF) or PCMCIA cards do not work in SAGE RTU CPUs.

Product:
SAGE Remote Terminal Units (RTUs) — CPU modules that use CF/PCMCIA storage media.

Environment:
RTU CPU requiring a CF or PCMCIA card; media prepared by manually copying files via a card reader (no factory programming).

Cause:
Off‑the‑shelf CF/PCMCIA cards lack the special boot routine stored in Sector 0 (boot sector) that the SAGE RTU CPU requires to initialize. This boot sector is not created or replicated by simply copying files using a card reader, resulting in a non‑bootable card.

Resolution:

  • Use factory‑programmed media: Install CF/PCMCIA cards that are pre‑programmed for SAGE RTUs. Example: CF part number C3414‑S02‑10001.
  • Do not clone by file copy: Avoid preparing cards by copying files; this does not reproduce the required boot sector.
  • Procurement: Contact an authorized distributor or your SAGE RTU support representative to obtain compatible, pre‑configured cards.
  • After installation: Insert the factory‑programmed card into the RTU CPU and power‑cycle to confirm proper initialization.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings