Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
RADIUS Secret minimum character limit when using RADIUS message authenticator

Issue

Customers require a minimum of 8 characters for their RADIUS secret on NMC2 devices when using the message authenticator setting.

Product Line

  • Network Management Card 2 - AP9630/30CH, AP9631/31CH, AP9635/35CH
    Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.

Environment

Firmware v7.2 and higher

Resolution

Schneider Electric has added a new RADIUS setting as of firmware version 7.2.0 called the RADIUS Message Authenticator.  In order to use the RADIUS Message Authenticator the RADIUS Secret must now be configured for a minimum of 8 characters.

Configuration of the RADIUS secret can be done through the following methods:

  • Web User Interface (UI) – Configuration/Security/Remote Users/RADIUS.
    • Click on the IP address hyperlink for the Primary RADIUS server you are configuring.

web ui

    • Enter the RADIUS secret (minimum 8 characters in length) under the Secret section.

web ui

    • Click Apply.
    • Repeat this step for the Secondary RADIUS server if necessary.
  • Command Line Interface (CLI) – Accessible via the console port or Telnet/SSH.
    • To configure the RADIUS secret for the primary or secondary server use the following syntax. Note: The RADIUS secret must be a minimum of 8 characters.
      • radius -s1 <RADIUS secret> then <enter>.

radius -s2 <RADIUS secret> then <enter>