Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to control an ATV Drive using a HMIST6 with Modbus TCP?

Issue

Trying to control an ATV Drive with an HMIST6 without using a PLC via Modbus TCP

Product Line

HMIST6 HMI Family

ATV Drives Family

Environment

SoMove

EcoStruxure Operator Terminal Expert

Resolution

A) ATV Drive Setup in SoMove

1. On the SoMove project assign a Fixed IP address.

2. Set a Drive Modbus Address, it can be 1. If more than one drive is being used, make sure every drive has a different address number.

3. Set the protocol configuration to "Modbus TCP" if there is more than one protocol option.

4. Set the control mode configuration CHCF to "I/O mode".

B) HMI Setup in EOTE

1. Add a Modbus TCP Master driver.

Adding Driver

2. Set the IP address and Equipment Address to match the configuration on the ATV Drive.

Driver Configuration

3. Under variables, add the variables manually. Use the Logic Address information that matches the ATV Drive being used.

Example:

Variables

4. Bind the variables to the screen objects.

5. Download the projects and test.

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: