How can we help you today?

Which SNMP OID can I use to display the APC Network Management Card information?

Issue:
Looking for the SNMP OID to display the Network Management Card information.

Product:
APC Network Management Cards and Network Managed Devices - All Serial Numbers


Answer:

The OID 1.3.6.1.2.1.1.1.0 corresponds to the sysDescr object in SNMP (Simple Network Management Protocol). This object provides the following textual description of a network device’s system:

  • Details about its hardware - (Model / SKU and Serial Number)
  • Firmware - (APC Operating System, Application Module, and Boot Monitor if Applicable to the model)

Below is an example of what data it will give once polled in an SNMP browser :

The following image shows a screen shot from an SNMP browser using the object name sysDescr OID

Please contact our Technical Support Agents at 1-800-800-4272 or chat with us at APC by Schneider Electric for any clarifications or questions.

Schneider Electric Nigeria