How can we help you today?

How to Upload New User Packages and Manage Roles on SAGE RTU

Issue:

Need to add, update, or delete user accounts and assign roles for secure access to RTU functions.

Product:

SAGE Remote Terminal Unit (RTU)

All Models

Environment:

  • Firmware version C3414-500-S02YZ or later
  • User Manager utility installed on PC
  • Access to RTU web GUI with Up/Download privileges

Cause:

Default user credentials (Admin/Telvent1!) are insecure and must be replaced. Role-based access control ensures compliance and limits unauthorized actions.

Resolution:

  1. Create User Package with User Manager:

    • Launch User_Manager_YZ.exe from firmware update package.
    • Add users:
      • Username: ≥5 characters, no special characters
      • Password: ≥8 characters, includes uppercase, lowercase, number, punctuation
    • Assign Role (Config, Display, Command, Up/Download, File Transfer, Remote Shell, IED Tunnel).
    • Optionally attach SSH public key (.pk2) for secure services.
    • Click Generate to create:
      • <DESC>_<VER>_Users.tar.gz (upload file)
      • access_<DESC>_<VER>.cfg (backup/recovery file)
  2. Upload User Package to RTU:

    • Log in to RTU web GUI with Up/Download privilege.
    • Navigate to Up/Download → Update Users.
    • Click Choose File, select .tar.gz package, then Send to RTU.
    • Changes apply immediately; no reboot required.
  3. Manage Roles and Sessions:

    • Max 5 concurrent logins; session timeout configurable (default 15 min, max 180 min).
    • Proper logout required to avoid lingering sessions.
  4. Password Recovery:

    • Import access_<DESC>_<VER>.cfg in User Manager if password not concealed.
    • Concealed passwords cannot be recovered.

Schneider Electric Nigeria